earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Server, Virtual Project Servers
Functionalities: User Management
Product version: 1.8
10/13/2016

Workspace – Content Tab

Use the Content tab to edit the content and layout of a workspace.

 
action_zoom_plus_stroke Content tab
Figure: Content tab

Table: Content Tab

Component

Description

Menu

Select Visible to show the menu in the workspace.

Address bar

Select Visible to show the address bar in the workspace.

Search bar

Select Visible to show the search bar in the workspace.

Toolbar

Select Visible to show the toolbar in the workspace.

Status bar

Select Visible to show the status bar in the workspace.

History bar

Select Visible to show the history bar in the workspace.

Root path (Applies to Address Bar and System Tree)

Displays the path to the basic node of the workspace. For more information, see Workspace Content References .

 
action_zoom_plus_stroke

Add

Click to open the Create Object Wizard, where you add a new component to the workspace. For more information, see Create Object Wizard – Naming the Object Page .

 
action_zoom_plus_stroke

Edit

Click to edit a pane. For more information, see Pane Properties .

 
action_zoom_plus_stroke

Remove

Click to remove a component.

  • Workspace Components and Customization
  • Workspace – Summary Tab
  • Workspace – Members Tab
  • Create Object Wizard – Naming the Object Page
  • Workspace Content References