earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Conceito

Conceito


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Gestão de utilizadores
Versão do produto: 3.2, 3.3, 2022
15-10-2020

WorkStation Account Validation

All user account information is stored centrally in the EcoStruxure Building Operation user database, which contains information about software permissions, user account memberships, workspaces, and domains.

Account Validation

When you log on to WorkStation you have to quote your user name and password together with the domain and EcoStruxure BMS server you want to log on to. The EcoStruxure Building Operation software confirms that you are using a valid user account and verifies that correct password is used. The EcoStruxure Building Operation software also authenticates access to workspaces associated with your user account group memberships. After validation, the EcoStruxure Building Operation software retrieves your software permissions and stores them in a user token, valid for this log on session.

Nota

User name, password, and domain name are case sensitive.

WorkStation User Token

A user token remains active as long as you are logged onto WorkStation. Any changes to your software permissions during your current sessions take effect the next time you log on.

  • Iniciar sessão em WorkStation como outro utilizador Windows
  • Iniciar sessão em WorkStation como utilizador EcoStruxure Building Operation
  • WorkStation Account Management
  • User Accounts and User Account Groups
  • User Account Management Overview