WorkStation is your main interface to your EcoStruxure BMS. You use WorkStation to perform all work on a daily basis in the EcoStruxure BMS.
You log on to WorkStation to securely access the functions in WorkStation. You log on to WorkStation as a Windows user or an EcoStruxure Building Operation user. Your system administrator decides which type of user you log on as.
For more information, see Log on to WorkStation or WebStation .
As the owner, you register your EcoStruxure BMS to ensure that you are informed of the latest product news, relevant offers, and system updates. This information enables you to optimize maintenance and functionality of your system, protect asset value, and produce a healthier building for optimal comfort conditions.
For more information, see System Registration .
The Work area in the EcoStruxure Building Operation user interfaces may vary depending on how it is set up. A typical EcoStruxure Building Operation workspace contains panes and views.
For more information, see User Experience .
In WorkStation you can customize your workspace to some extent. You can, for example, decide where workspace components, such as, Alarms are displayed.
For more information, see Customization .
To get a better view of the objects in views and lists, you can use a number of functions like filtering, grouping, and sorting.
For more information, see Basic Functions .
You can change and force values using a graphic or the Properties pane. Using the Watch pane in WorkStation, you can dynamically monitor a value.
For more information, see Modify Values .
You are notified by alarms when some important event occurs. For example, if the temperature is too low or too high in a building, if a window is open, or if something is broken, such as a fan. The system administrator sets up the alarms and decides to whom the alarm is sent.
For more information, see How Alarms Work .
All system events, as well as information and circumstances, are recorded in the Event log. These event records can be viewed in the Events pane or in an Event View.
For more information, see How Events Work .
Schedules are used to schedule the operation of part of the building management system, such as a fan, a door, or a setpoint. Using a schedule, a fan can be set to operate between 08:00 and 17:00 every workday.
For more information, see How Schedules Work .
You use trend logs to record values, such as a sensor. A trend log can also log consumptions, such as energy consumption or water consumption.
For more information, see How Trend Logs Work .
You use graphics to display building overviews, display values from sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.
For more information, see How Graphics Work .
You can open documents stored on an EcoStruxure BMS server using the default program associated with the file type. For example, a txt-file opens Notepad and a ppt-file opens PowerPoint.
For more information, see How Documents Work .
WorkStation Help provides you with information on how to handle and understand the EcoStruxure BMS.
For more information, see WorkStation Help .