The Work area in the EcoStruxure Building Operation user interfaces may vary depending on how it is set up. A typical EcoStruxure Building Operation workspace contains panes and views.
The workspace in WorkStation and WebStation is the area where you perform all tasks at your site, such as acknowledging alarms and viewing trend logs.
For more information, see Workspaces .
A pane is a separate area in the workspace. You use panes to carry out commands, navigate the system or display information. Panes can be moved, hidden, closed, and repositioned.
For more information, see Different Layouts Using Panes .
To ease the daily operation, you can use shortcut keys to most of the commands inWorkStation.
For more information, see Keyboard Shortcuts for WorkStation .
You can navigate between the available open windows in the Work area. The windows you can select using the Window menu are represented by tabs in the Work area.
For more information, see Window Menu .