Use the Domain properties to configure the properties of a domain.
Component |
Description |
Maximum logon attempts |
Select the maximum number of failed logon attempts that a user can make before WorkStation is temporarily locked. |
Password |
Type the password SmartStruxure servers internally use to enhance the SmartStruxure server communication security in the domain. |
Confirm Password |
Type the password SmartStruxure servers internally use to enhance the SmartStruxure server communication security in the domain. |
Windows domain name |
Type the name of the Windows domain where the Windows Active directory is located from which you want to map user account groups. Para obtener más información, consulte Windows Active Directory User Groups . |