Produits : WebStation
Fonctionnalités : Fonctionnalité de base
Version produit : 2024, 7.0
03/12/2024

Changing Your Password

You change your EcoStruxure BMS user password on a regular basis to keep your information secure.

Afficher plus
action_close

You log on to WorkStation or WebStation to securely access the EcoStruxure BMS features.

Log on to WorkStation

You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure BMS user. Your system administrator decides which type of user you log on as. ​

To log on to WorkStation using an EcoStruxure BMS account, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.

The account information for both the EcoStruxure BMS account and the Windows account is provided by the system administrator.

Déclaration

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. Pour plus d'informations, voir EcoStruxure Building Operation Software Licensing Installation and Location .

Remember me on this computer

For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both BMS users and Windows users can use the Remember me feature.

Add a display name of the server address

When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.

Log on to WebStation

To log on to WebStation, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

The account information for your account is provided by the system administrator.

To change your password
  1. In WebStation, on the Settings menu, click Options and then click Change password .

  2. In the Change password dialog box, in the Old password box, type your old password.

  3. In the New password box, type your new password.

  4. In the Confirm password box, type your new password again.

  5. Click OK .

  • Log on to WorkStation or WebStation
  • Change Password Dialog Box
  • Logging On to WebStation
  • Logging Off WebStation