Produits : WebStation
Fonctionnalités : Fonctionnalité de base
Version produit : 2024, 7.0
02/12/2024

Logging On to WebStation

You log on to WebStation to access the EcoStruxure BMS database.

Afficher plus
action_close

You log on to WorkStation or WebStation to securely access the EcoStruxure BMS features.

Log on to WorkStation

You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure BMS user. Your system administrator decides which type of user you log on as. ​

To log on to WorkStation using an EcoStruxure BMS account, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.

The account information for both the EcoStruxure BMS account and the Windows account is provided by the system administrator.

Déclaration

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. Pour plus d'informations, voir EcoStruxure Building Operation Software Licensing Installation and Location .

Remember me on this computer

For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both BMS users and Windows users can use the Remember me feature.

Add a display name of the server address

When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.

Log on to WebStation

To log on to WebStation, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

The account information for your account is provided by the system administrator.

To log on to WebStation
  1. In WebStation, in the login view, in the User name box, type your user name.

  2. In the Password box, type your password.

  3. In the Domain box, type a domain name.

  4. Click Log on .

  • Log on to WorkStation or WebStation
  • Fenêtre Building Operation WebStation
  • Logging Off WebStation
  • Changing Your Password