earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Trends
Product version: 1.8, 1.9
6/25/2015

Showing Markers in a Trend Log Series

You show trend log series with markers for each record to make reading easier.

Note:

This feature is only applicable to lines and discrete lines.

Show More
action_close

Trend charts are a way to graphically present trend logs. A trend chart can contain one or more trend logs that are represented in the trend chart by lines or bars.

You can also add and remove trend logs from a trend chart. This makes it easy to compare different trend logs, for example the energy consumption compared to the average temperature.

 
action_zoom_plus_stroke Trend chart in WorkStation
Figure: Trend chart in WorkStation

Trend Chart Navigation in WorkStation

The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.

For more information, see Trend Chart Navigation in WorkStation .

Trend Chart Navigation in WebStation

The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.

For more information, see Trend Chart Navigation in WebStation .

Trend Chart Series in WorkStation

You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.

For more information, see Trend Chart Series in WorkStation .

Trend Chart Series in WebStation

You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.

For more information, see Trend Chart Series in WebStation .

Trend Chart Axes in WebStation

​A trend chart displays the records of a trend log or an extended trend log as a series.

For more information, see Trend Charts .

To show markers in a trend log series
  1. In WebStation, in the System Tree pane, select the trend chart.

  2. On the Trend Chart toolbar, click Settings .

  3. Click the Series tab.

  4. Select the series you want to display with markers.

     
    action_zoom_plus_stroke
  5. In the Show markers box, select True .

  6. Click OK .

The series is now presented with markers.

 
action_zoom_plus_stroke Trend chart showing one trend log series with markers and two without markers
Figure: Trend chart showing one trend log series with markers and two without markers
  • Trend Chart Series in WebStation
  • How Trend Charts Work
  • Displaying Specific Time Spans of a Trend Chart in WebStation
  • Changing the Line Weight of a Trend Chart Series
  • Changing the Color of a Trend Chart Series
  • Changing the Presentation Type of a Trend Chart Series
  • Viewing Multiple Tooltips in a Trend Chart
  • Adding a Trend Chart Series to a Trend Chart in WebStation
  • Removing a Trend Chart Series
  • Saving Current Trend Chart Settings
  • Trend Chart View
  • Trend Chart Settings Dialog Box – Series Tab