earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Trends
Product version: 1.8, 1.9
10/23/2015

Trend Chart Settings Dialog Box – Series Tab

Use the Series tab in WebStation to change the presentation of a series in a trend chart.

 
action_zoom_plus_stroke Series tab
Figure: Series tab

Table: Series Tab

Component

Description

Trend chart list

Displays the path to the trend chart series.

Series presentation

Select a presentation type for the series. The series can be presented with a line, a discrete line, digital, or bars. For more information, see Trend Series .

Assigned axis

Select Left to connect the series to the left y axis. Select Right to connect the series to the right y axis.

Weight

Type the weight of the line. The value has no correlation to any unit of measure.

Show markers

Select True to show a marker for each record. The marker can only be shown for lines and discrete lines, not for digital and bars.

Show events

Select True to show events.

Color

Select a color for the series.

  • Trend Chart Series in WebStation
  • Trend Series
  • Trend Chart Series Menu
  • Trend Chart Settings Dialog Box – Axis Tab
  • Trend Chart Settings Dialog Box – Calculation Tab