earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WebStation
Funktionaliteter: Tidsscheman
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Adding a Date Range Exception Event

You create a date range exception event to schedule a date range event that takes precedence over a scheduled weekly event.

Visa mer
action_close

An exception event occurs instead of the scheduled weekly events for a single date, date range, calculated date, or calendar reference.

For example, you create an exception event in March for an intense aerobics class in the gym to open an air vent to 100 % from 06:30 to 17:00 every Wednesday in March. This exception event takes precedence over the regularly scheduled weekly Wednesday events.

When scheduling exception events, you can use four exception types to provide flexibility and control in your schedule.

Date Exception Events

A single date exception event can occur on a single day, or you can use the options for the event to occur on more than one day. The options such as Any year and Any day provide flexibility. To schedule a single date event to take place every year on October 31, you select the following single date options:

  • Year: Any year

  • Month: October

  • Day of month: 31

  • Day of week: Any day

Date Range Exception Events

A date range exception event is an event that lasts over a period of time. In addition to a specific day of month, you can select Odd, Even , or Any month , and Any day or Last day , to provide the flexibility to a date range. For example, to schedule an exception event to occur annually from the last day of March to the last day of April, select the following options for the start and end dates:

Start Date
  • Start year: Any year

  • Start month: March

  • Day of month: Last day

  • Day of week: Any day

End Date
  • Year: Any year

  • Month: April

  • Day of month: Last day

  • Day of week: Any day

Calculated Exception Events

A calculated date is an exception event that recurs. Other than a specific month and week, you can select Any month and Any week or Last week , to provide flexibility to a calculated date. For example, to schedule the Monday of the first week of every month for an exception event, select the following options:

  • Month: Any month

  • Week of month: First week

  • Day of week: Monday

Calendar Exception Events

A calendar reference allows you to apply an exception event for all dates specified in the calendar. For example, to schedule exception events for all holidays on a calendar, you select the calendar you want to reference and the schedule will follow the holidays created in the calendar.

To add a date range exception event
  1. In WebStation, in the System tree pane, select the schedule you want to add the date range exception event to.

  2. Select Add exception .

  3. In the Schedule event properties dialog box, click All day to have the exception event on all day.

  4. In the Value box, enter the value for the exception event.

  5. In the At box, enter the start time for the exception event.

  6. In the Until box, enter the end time for the exception event.

  7. In the Exception name box, type a name for the exception event.

  8. In the Exception priority box, enter the priority for the exception event.

  9. Under Date , in the Exception type box, select Date range .

  10. Enter the year, month, week, and day you want the exception event to start.

  11. Enter the year, month, week, and day you want the exception event to end.

  12. Click OK .

  13. Click Save .

  • Exception Events in WebStation
  • Weekly Events in WebStation
  • Schedule Editor in WebStation
  • Schedule Workspace
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Editing a Date Range Exception Event
  • Adding a Single Date Exception Event
  • Adding a Calculated Exception Event
  • Adding a Calendar Exception Event
  • Adding a Weekly Event