earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: WebStation
Funktionaliteter: Tidsscheman
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Schedule Event Properties Dialog Box – Single Date Exception View

Use the Single Date Exception View in the Schedule Event Properties dialog box to schedule a single date exception.

 
action_zoom_plus_stroke Schedule event properties dialog box – Single date exception view
Figur: Schedule event properties dialog box – Single date exception view

Tabell: Schedule Event Properties Dialog Box – Single date Exception View

Component

Description

All Day

Select to create an all day event.

Value

Enter a value for the exception event.

At

Enter the start time for the exception event.

Until

Enter the end time for the exception event.

Exception name

Type a name for the event.

Exception priority

Select a priority number between 1 (highest priority) and 16 (lowest priority).

Event type

Select Single date .

Year

Enter the year for the single date event.

Month

Enter the month for the single date event.

Day of month

Enter the day of month for the single date event.

Day of week

Enter the day of week for the single date event.

  • Exception Events in WebStation
  • Schedule Event Properties Dialog Box – Weekly View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Calculated Exception View
  • Schedule Event Properties Dialog Box – Calendar Reference View