earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos Enterprise Server, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.8, 1.9
13/10/2016

Deleting a Backup Set from the Enterprise Server

You delete a backup set from the db_backup folder of the Enterprise Server when you no longer need the backup set.

Mostrar más
action_close

Backup sets are compressed backup files used for restoring data. Building Operation stores the local backup set for an Enterprise Server or SmartStruxure server devices in the Local folder within the Backup sets folder.

Backup Sets Location

Backup sets are stored in different locations for stand-alone systems and multi-server systems.

Para obtener más información, consulte Location of Backup Sets .

Backup Sets and Server Name

Building Operation associates each backup set with a particular SmartStruxure server name. Therefore, you should not rename a SmartStruxure server unless absolutely necessary. If you do rename a SmartStruxure server, the previous backup sets do not display in the Restore Options dialog box. You can view all the backup sets that are stored locally on an Enterprise Server. Para obtener más información, consulte Locating the Local Backup Path on the Enterprise Server .

Aviso

Going forward, you must create new backups for the renamed SmartStruxure server.

Backup Set Storage and Protection

SmartStruxure servers store backup sets in their local directories. By design, the average user may not easily locate these backup directories using a Windows-based file system. For convenience, you can save backup sets stored on SmartStruxure servers to WorkStation. After saving the backup set, you can also copy the file to another backup storage location.

Para obtener más información, consulte Backup Set Storage and Protection .

Backup Set Import from WorkStation

You import a backup set from WorkStation to replace a lost or incomplete backup set, or to add a backup set to a new SmartStruxure server.

Para obtener más información, consulte Backup Set Import from WorkStation .

Automatic Purge of Backup Sets

An Enterprise Server stores multiple local and remote backup sets. As a result, these sets can consume much needed space on the Enterprise Server. To resolve this problem, you can configure the Enterprise Server to remove outdated backup sets.

Para obtener más información, consulte Automatic Purge of Backup Sets .

To delete a backup set from the Enterprise Server
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the Enterprise server.

     
    action_zoom_plus_stroke
  3. Click Backup and Restore Manager .

  4. In the Backup sets path box, copy the entire backup sets path of the Enterprise Server.

     
    action_zoom_plus_stroke
  5. Open a browser, such as Windows Explorer.

  6. In the browser Address box, paste the backup sets path and press Enter .

  7. In the db_backup folder, open the ASArchives or LocalBackup folder.

     
    action_zoom_plus_stroke
  8. Right-click on the backup set that you want to delete and click Delete .

  9. Click Yes to remove the backup set.

     
    action_zoom_plus_stroke
  • Backup Sets
  • Backup Set Storage and Protection