SmartStruxure servers store backup sets in their local directories. By design, the average user may not easily locate these backup directories using a Windows-based file system. For convenience, you can save backup sets stored on SmartStruxure servers to WorkStation. After saving the backup set, you can also copy the file to another backup storage location.
Saving a backup set to a storage location is a two-step process: saving the backup set and then relocating the file to another location. First, you save the backup set to WorkStation. Second, you copy the backup set from WorkStation to another storage location on your network, such as a USB drive.
To save time, you can create a uniquely named directory in which to store your saved backup sets for a particular SmartStruxure server. This unique folder name can help you identify a particular Enterprise Server or SmartStruxure server device backup set, such as AS-1 Final Configuration Backup. Using this method, you can easily locate the backup set on your network.
Scheduled backup sets have a unique file name and extension based on the date stamp and server name. However, you can rename the backup set, if necessary. Para obtener más información, consulte Scheduled Backups .
You can remove backups sets in two ways:
Manually: You can delete backups sets using a browser. Para obtener más información, consulte Deleting a Backup Set from the Enterprise Server .
Periodically: You can configure the system to remove backup sets on a regular basis. Para obtener más información, consulte Automatic Purge of Backup Sets .