earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Modalità

Modalità


Prodotti: Enterprise Server, Project Configuration Tool
Funzionalità: Funzionalità di base
Versione del prodotto: 1.8, 1.9
13/10/2016

Deleting a Backup Set from the Enterprise Server

You delete a backup set from the db_backup folder of the Enterprise Server when you no longer need the backup set.

Mostra di più
action_close

Backup sets are compressed backup files used for restoring data. Building Operation stores the local backup set for an Enterprise Server or SmartStruxure server devices in the Local folder within the Backup sets folder.

The SmartStruxure server device stores only one backup set at a time, so each new backup operation overwrites the previous backup set. However, an Enterprise Server can store multiple backup sets locally.

 
action_zoom_plus_stroke Backup sets in the Local folder
Figura: Backup sets in the Local folder

Unlike a SmartStruxure server device, an Enterprise Server can store multiple local and remote backup files. In multiple server sites, the Enterprise Server manages all the SmartStruxure server devices in its group. Consequently, the backup set is actually stored in two places: on the SmartStruxure server devices and on the Enterprise Server. In the Backup sets folder of the installation directory, Building Operation creates two directories:

  • ASArchives : Lists separate subfolders that reflect the name of each SmartStruxure server device. Each subfolder contains the backup files for that SmartStruxure server device.

  • LocalBackup : Lists all the local backup files for the Enterprise Server.

SmartStruxure Server Rename

Building Operation associates each backup set with a particular SmartStruxure server name. Therefore, you should not rename a SmartStruxure server unless absolutely necessary. If you do rename a SmartStruxure server, the previous backup sets do not display in the Restore Options dialog box. You can view all the backup sets that are stored locally on an Enterprise Server. Per maggior informazioni, consulta Locating the Local Backup Path on the Enterprise Server .

Avviso

Going forward, you must create new backups for the renamed SmartStruxure server.

Backup Set Storage and Protection

SmartStruxure servers store backup sets in their local directory. By design, the average user may not easily locate these backup directories using a Windows-based file system. For convenience, you can save backup sets stored on SmartStruxure servers to WorkStation. After saving the backup set, you can also copy the file to another backup storage location.

Per maggior informazioni, consulta Backup Set Storage and Protection .

Backup Set Import from WorkStation

You import a backup set from WorkStation to replace a lost or incomplete backup set, or to add a backup set to a new SmartStruxure server.

Per maggior informazioni, consulta Backup Set Import from WorkStation .

Automatic Purge of Backup Sets

An Enterprise Server stores multiple local and remote backup sets. As a result, these sets can consume much needed space on the Enterprise Server. To resolve this problem, you can configure the Enterprise Server to remove outdated backup sets.

Per maggior informazioni, consulta Automatic Purge of Backup Sets .

To delete a backup set from the Enterprise Server
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the Enterprise server.

     
    action_zoom_plus_stroke
  3. Click Backup and Restore Manager .

  4. In the Backup sets path box, copy the entire backup sets path of the Enterprise Server.

     
    action_zoom_plus_stroke
  5. Open a browser, such as Windows Explorer.

  6. In the browser Address box, paste the backup sets path and press Enter .

  7. In the db_backup folder, open the ASArchives or LocalBackup folder.

     
    action_zoom_plus_stroke
  8. Right-click on the backup set that you want to delete and click Delete .

  9. Click Yes to remove the backup set.

     
    action_zoom_plus_stroke
  • Backup Sets
  • Backup Set Storage and Protection