earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Modalità

Modalità


Prodotti: Enterprise Server, Project Configuration Server, Project Configuration Tool
Funzionalità: Funzionalità di base
Versione del prodotto: 1.8
13/10/2016

Locating the Local Backup Path on the Enterprise Server

You locate the local backup folder on the Enterprise Server to view the stored backup sets. The system displays the valid backup sets stored in this folder in the Restore Options dialog box.

Mostra di più
action_close

SmartStruxure servers store backup sets in their local directory. By design, the average user may not easily locate these backup directories using a Windows-based file system. For convenience, you can save backup sets stored on SmartStruxure servers to WorkStation. After saving the backup set, you can also copy the file to another backup storage location.

Saving a backup set to a storage location is a two-step process: saving the backup set and then relocating the file to another location. First, you save the backup set to WorkStation. Second, you copy the backup set from WorkStation to another storage location on your network, such as a USB drive.

 
action_zoom_plus_stroke Copy backup set from a SmartStruxure server to a network drive
Figura: Copy backup set from a SmartStruxure server to a network drive
Uniquely Named Storage Directory

To save time, you can create a uniquely named directory in which to store your saved backup sets for a particular SmartStruxure server. This unique folder name can help you identify a particular Enterprise Server or SmartStruxure server devices backup set, such as AS-1 Final Configuration Backup. Using this method, you can easily locate the backup set on your network.

Backup Set Renaming

Scheduled backup sets have a unique file name and extension based on the date stamp and software version. However, you can rename the backup set, if necessary. Per maggior informazioni, consulta Scheduled Backups .

Backup Set Removal

You can remove backups sets in two ways:

To locate a local backup path on the Enterprise Server
  1. In WorkStation, in the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the Enterprise server.

     
    action_zoom_plus_stroke
  3. Click Backup and Restore Manager .

  4. In the Backup sets path box, view the local backup path on the Enterprise server.

     
    action_zoom_plus_stroke
  • Restoring the SmartStruxure Server
  • Backup and Restore Manager on the Enterprise Server
  • Backup Set Storage and Protection