earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Modalità

Modalità


Prodotti: WorkStation
Funzionalità: Allarmi, Funzionalità di base
Versione del prodotto: 1.8
15/11/2017

Determining the Alarm State Sort Order

You use the Alarm state sort order dialog box to determine in what order the alarms are sorted when the column State is used for sorting the alarms in the Alarms pane or an Alarm View.

Mostra di più
action_close

​An alarm is always in a certain alarm state. The state of the alarm is presented in the alarm properties, in the Alarms pane, or in the Alarm Views.

Tabella: Alarm States

Alarm State

Description

Normal state

Idle state where the alarm monitors the variable. Normal state = 0.

Alarm state

When an alarm is triggered, the state of the alarm changes from the normal state to alarm state. Alarm state = 1.

Acknowledge state

A user or user group has acknowledged the alarm. Acknowledged state = 2.

Reset state

The monitored variable has returned to a value that is within the normal condition of the alarm, but the alarm has to be acknowledged by a user before the alarm returns to normal state. Reset state = 3.

Disable state

You can disable an alarm when the alarm is triggered by faulty reasons, the alarm toggles between the alarm state and reset state, or maintenance will trigger the alarm. Disabled state = 4.

A Disabled alarm can be hidden in the Alarms pane or Alarm Views. To reset the alarm, you have to show hidden alarms and then enable it. When you show disabled alarms, enabled alarms are hidden.

Fault state

If a BACnet device reports values that it knows are not trustworthy, the monitoring alarm is put in fault state. Fault state = 5.

You can configure the alarm in different ways whether or not a user has to acknowledge the alarm before it returns to normal state.

Per maggior informazioni, consulta Acknowledgements .

Alarm Handling Issues

When an alarm is triggered it appears in the alarm list. You can acknowledge, disable, or hide alarms in the alarm list. An acknowledged alarm disappears from the alarm list when it has been reset to normal state.

Per maggior informazioni, consulta Alarm Handling Issues .

To determine the alarm state sort order
  1. In WorkStation, right-click in the Alarms pane or in an Alarm View.

  2. Point to Alarm View settings and then click Alarm state sort order .

     
    action_zoom_plus_stroke
  3. Select the state you want to reposition with respect to the other states.

     
    action_zoom_plus_stroke
  4. Click the up or down arrow to change the sort order.

  5. Repeat the repositioning on other states.

  6. Click OK .

When you click the State column heading in the Alarms pane or an Alarm View, the alarms are sorted in the order specified in the Alarm state sort order dialog box. Another click reverses that order.

  • Alarm States
  • Alarms Pane and Alarm View Icons
  • Alarms Pane Shortcut Menu