earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : WebStation
Fonctionnalités : Tendances
Version produit : 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
14/03/2024

Axes d'une courbe de tendance dans WebStation

The x-axis of the trend chart represents time. The time span of the axis can be set with a fixed start and end time or with an end time relative to the present time. The axis can be quick-scaled to show the last hour, last day, last month, or last year​.

 
action_zoom_plus_stroke Absolute time span and relative time span, schematic
Figure : Absolute time span and relative time span, schematic

The y-axis refers to the measurement unit that the variable represents. The scale of the y-axis can be set manually or by auto scale. You can configure the trend chart to present series on one y-axis or two y-axes, one to the left and one to the right. Use two y-axes to present series with different ranges in the same trend chart.

 
action_zoom_plus_stroke One y-axis and two y-axes, schematic
Figure : One y-axis and two y-axes, schematic

To make reading easier, grid lines can be shown in the trend chart. Grid lines can be shown in both the x- and y-direction, independent of each other.

 
action_zoom_plus_stroke Grid lines, schematic
Figure : Grid lines, schematic
  • Trend Charts
  • Comment fonctionnent les courbes de tendance
  • Mode de fonctionnement des journaux de tendance
  • Vue de courbe de tendance
  • Trend Chart Toolbar
  • Boîte de dialogue Configurer courbe de tendance – Onglet Axe X
  • Configuration de l'axe X avec une période relative
  • Configuration de l'axe X avec une période absolue
  • Affichage du quadrillage de la courbe de tendance
  • Configuration manuelle de l'échelle de l'axe Y
  • Configuration automatique de l'échelle de l'axe Y