Log on to rate and give feedback
12345Log on to rate
0
How to
Products:
WebStation
Functionalities:
Trends
Product version:
1.8, 1.9
6/25/2015
Zooming In and Out of a Trend Chart
You zoom in a trend chart to make the reading easier.
Show More
action_close
The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.
You can zoom in or out on the x axis, the y axis, or both axes, or zoom in a specific area of the trend chart. Use the zoom to fit function to automatically adjust the trend chart x axis and y axis according to the range of the series displayed.
To zoom in and out of a trend chart
In WebStation, in the
System Tree
pane, select the trend chart.