earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Server, Virtual Project Servers
Functionalities: Trends
Product version: 1.8
10/13/2016

Mass Creating Extended Trend Logs

You use the mass create feature to create identical extended trend logs from trend logs, instead of creating the extended trend logs one by one.

Show More
action_close

You use the mass create feature to create multiple identical alarms or trend logs for different objects, instead of creating the alarms or trend logs one by one. From trend logs, you can mass create extended trend logs.

The main principle in Building Operation is that what you can do from one object or property, you can mass create from a number of selected objects or properties on a one to one basis. For example, you have seven objects that you want to monitor with seven interval trend logs. By selecting the objects and starting the ordinary New Object wizard, you configure a generic interval trend log template. When finishing the wizard Building Operation automatically creates seven identical interval trend logs that monitor individual objects.

 
action_zoom_plus_stroke Mass creating identical trend logs from different variables.
Figure: Mass creating identical trend logs from different variables.

Object or Property Variable Type

In Building Operation, you can create alarms or trend logs that are suitable for the variable type you have selected.

For more information, see Object or Property Variable Type .

Suffix and Prefix

When you mass create objects you can specify a prefix and suffix that are added to the created object name. The prefix is added before the name and the suffix is added after.

For more information, see Suffix and Prefix .

Mass Create Unit Management

You can only mass create alarms with identical units or no unit. When you mass create trend logs, each trend log gets the same unit as the logged variable.

For more information, see Mass Create Unit Management .

Mass Create from Properties with the Search Method

Mass creating can be performed by either selecting objects in the object list or selecting the objects or properties in a search result list. Using the search result list is very convenient if you want to monitor a number of properties located in different devices or folders. For example, you want to create enumeration alarms that monitor the reliability property on several I/O points. The I/O points are located on several SmartStruxure server devices By performing a search for the reliability property you can select the points that you want to monitor in the search result list.

Mass Create Path Options

You have three options when deciding where to create new alarms, trend logs, and extended trend logs:

  • The same folder as each selected object

  • A different folder, relative to the path of each selected object

  • A single folder for all created objects

To mass create extended trend logs
  1. In Workstation, in the List View, select the trend logs that you want to create extended trend logs for.

     
    action_zoom_plus_stroke
  2. On the File menu, point to New and then click Extended Trend Log .

  3. In the Prefix box, type a label that is added in front of the name of the extended trend logs.

     
    action_zoom_plus_stroke
  4. In the Suffix box, type a label that is added after the name of the extended trend logs.

  5. In the Description box, type a description for the extended trend logs.

  6. In the Destination box, enter the destination where you want to create the trend logs. If you use A different folder, relative to the selected object , this destination applies to the first object in the list, and its path works as a pattern for the relative path that is applied to all the remaining objects.

    Note:

    If the specified relative path pattern leads to an unavailable position for any of the objects in the list, Next and Create are disabled.

  7. Click Next .  

For more information, see Creating an Extended Trend Log .

  • Mass Create
  • Object or Property Variable Type
  • Extended Trend Logs
  • Mass Creating Extended Trend Logs Using the Search Method
  • Cannot Mass Create Trend Logs or Alarms
  • Mass Create Unit Management
  • Mass Create Path Options
  • Creating an Extended Trend Log
  • Create Object Wizard – Naming the Object Page