earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface utilisateur

Interface utilisateur


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Alarmes
Version produit : 2.0, 2.1, 3.0, 3.1
18/12/2018

Create Variable Status Alarm Wizard – Alarm Trigger Page

Use the Alarm Trigger page to configure the trigger settings of the variable status alarm.

 
action_zoom_plus_stroke Variable status alarm trigger page
Figure : Variable status alarm trigger page

Table : Variable Status Alarm Trigger Page

Component

Description

Forced

Select to trigger the alarm when the monitored variable status is forced. Pour plus d'informations, voir Boutons Forcer et Déforcer .

Overridden

Select to trigger the alarm when the monitored variable status is overridden. Pour plus d'informations, voir Output Override Status .

Monitored variable

​Enter the path to the variable that is monitored by the alarm.

Disable alarm

Select to disable the alarm, for example, before deployment.

Alarm delay

​Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset.

Reset delay

​Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered.

Shunt variable 1

​Enter the shunt variable that is used to enable or disable the alarm. Pour plus d'informations, voir Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Pour plus d'informations, voir Shunt Variables .

Operator

Select AND or OR to add logic between the first and the second shunt variable. Pour plus d'informations, voir Shunt Variables .

Shunt variable 2

​Enter the second shunt variable that is used to enable or disable the alarm. Pour plus d'informations, voir Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Pour plus d'informations, voir Shunt Variables .

  • Create Alarm Wizard – Presentation Page
  • Create Alarm Wizard – User Action Page
  • Create Alarm Wizard – Attachment Page
  • Variable Status Alarm Properties – Basic Tab
  • Create Object Wizard – Naming the Object Page
  • Variable Status Alarms