Use the Alarm Trigger page to configure the trigger settings of the variable status alarm.
|
Component |
Description |
|
Forced |
Select to trigger the alarm when the monitored variable status is forced. Więcej informacji zawiera Force and Unforce Buttons . |
|
Overridden |
Select to trigger the alarm when the monitored variable status is overridden. Więcej informacji zawiera Output Override Status . |
|
Monitored variable |
Enter the path to the variable that is monitored by the alarm. |
|
Disable alarm |
Select to disable the alarm, for example, before deployment. |
|
Alarm delay |
Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset. |
|
Reset delay |
Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered. |
|
Shunt variable 1 |
Enter the shunt variable that is used to enable or disable the alarm. Więcej informacji zawiera Shunt Variables . |
|
Invert |
Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Więcej informacji zawiera Shunt Variables . |
|
Operator |
Select AND or OR to add logic between the first and the second shunt variable. Więcej informacji zawiera Shunt Variables . |
|
Shunt variable 2 |
Enter the second shunt variable that is used to enable or disable the alarm. Więcej informacji zawiera Shunt Variables . |
|
Invert |
Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Więcej informacji zawiera Shunt Variables . |