Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2022-07-12

Creating a Checklist

You create a checklist to connect it to an alarm, and to guide the user when troubleshooting a triggered alarm.

Pokaż więcej
action_close

A checklist is a set of steps that guides the user to which action to take when an alarm is triggered. If an alarm goes to normal state, the corresponding checklist is also reset and each step has to be checked again.

Checklists can be voluntary or mandatory. You can force the user to check each step in the checklist before the alarm can be acknowledged.

To create a checklist
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Checklists .

  4. In the Alarm Control Panel , in the Checklist view, click the Add checklist button

     
    action_zoom_plus_stroke
    .

  5. In the Add Checklist dialog box, in the Name box, type the name of the new checklist.

  6. In the Description box, type a description for the checklist.

  7. Click the Add step button

     
    action_zoom_plus_stroke
    .

  8. In the Add Checklist Step dialog box, in the Name box, type the text for the step to create.

  9. Click OK.

    Uwaga
    • You can add several steps to the checklist.

  10. In the Add Checklist dialog box, click OK .

  11. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Checklists View
  • Configuring Forced User Actions
  • Adding a Checklist to an Alarm
  • Editing a Checklist
  • Import and Export of Supporting Objects