earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2022-07-13

Adding a Checklist to an Alarm

You add a checklist to an alarm to troubleshoot the problem that triggered the alarm.

Pokaż więcej
action_close

A checklist is a set of steps that guides the user to which action to take when an alarm is triggered. If an alarm goes to normal state, the corresponding checklist is also reset and each step has to be checked again.

Checklists can be voluntary or mandatory. You can force the user to check each step in the checklist before the alarm can be acknowledged.

To add a checklist to an alarm
  1. In WorkStation, in the System Tree pane, select the alarm object to which you want to add a checklist.

  2. In the User Action tab, in the Checklist box, enter the checklist you want to add to the alarm.

  3. Click the Save button

     
    action_zoom_plus_stroke
    .

To add a checklist to an alarm, you must have created one in advance and defined its content.

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Checklists View
  • Configuring Forced User Actions
  • Adding a Checklist to an Alarm
  • Editing a Checklist
  • Creating a Checklist
  • Import and Export of Supporting Objects