Use the Objects and trends dialog box to view trend objects that are related to one or several selected objects or object properties.
Property |
Description |
[Quick filter] |
Enter a word or a character to filter on. For more information, see Quick Filter . |
Objects |
Lists the available objects, for example, the bound properties of a graphic component. |
Trends |
Lists the trends related to the selected object or property |
Path |
Displays the path of the object, property, or trend selected in the list. |