earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 3.2, 3.3, 2022
10/15/2020

Objects and Trends Dialog Box

Use the Objects and trends dialog box to view trend objects that are related to one or several selected objects or object properties.

 
action_zoom_plus_stroke Objects and trends dialog box when you have selected only one object or property.
Figure: Objects and trends dialog box when you have selected only one object or property.
 
action_zoom_plus_stroke Objects and trends dialog box when you have selected several objects, properties, or graphic components or groups containing bound properties.
Figure: Objects and trends dialog box when you have selected several objects, properties, or graphic components or groups containing bound properties.

Table: Objects and Trends

Property

Description

[Quick filter]

Enter a word or a character to filter on. For more information, see Quick Filter .

Objects

Lists the available objects, for example, the bound properties of a graphic component.

Trends

Lists the trends related to the selected object or property

Path

Displays the path of the object, property, or trend selected in the list.

  • Quick Filter