earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: WebReports
功能: 报告
产品版本: 1.8, 1.9
2017/9/22

WebReports Installation Overview

EcoStruxure Building Operation WebReports is installed using an installation package. Before you install WebReports, you must ensure that the computer on which you want to install WebReports (the Reports Server) meets the hardware and software requirements for WebReports, and that you have installed or enabled certain prerequisite items of software. These requirements are covered in the installation workflow (introduced in this topic).

WebReports Installer and WebReports Components

The WebReports Installer is a custom installer program that performs installation, prevalidation, and configuration of WebReports components. The WebReports Installer is delivered in an installation package, and the installation package has the format SE.SBO.WebReports-x.x.xxxxx.xxxx.exe. When you run the installation package, the WebReports Installer and accompanying files are placed in /Program Files (x86)/Schneider Electric StruxureWare/Building Operation WebReports Installation by default. The WebReports Installer will automatically run to install the WebReports when you run the installation package.

有关更多信息,请参阅 WebReports Installer and WebReports Components .

Reports Server Configuration

Install WebReports on the Reports Server, which is the computer where you install SQL Server.

有关更多信息,请参阅 Reports Server Configuration .

WebReports Installation WorkFlow

The WebReports installation workflow provides a guide to overall WebReports installation.

有关更多信息,请参阅 WebReports Installation WorkFlow .

Windows Roles and Features

The WebReports installation requires you to select certain roles and services to install on the Application Server and the Web Server (IIS), and to install .NET Framework 3.5 and .NET Framework 4.5 features. You install these roles and features using the Server Manager in Windows Server 2008, Windows Server 2012, or Windows Server 2012 R2. For Windows 7, Windows 8.1, and Windows 10, you configure IIS using Control Panel. It is recommended that you install these roles and features before you install SQL Server.

有关更多信息,请参阅 Windows Roles and Features .

SQL Server

SQL Server provides the platform for the Reporting Services database and the Reports database. You cannot install WebReports until you first create your Reports Server by installing a supported version of SQL Server.

有关更多信息,请参阅 SQL Server .

SQL Server Installation Settings

Before you can install WebReports successfully, it is imperative that the SQL Server has been installed with a particular group of settings.

有关更多信息,请参阅 SQL Server Installation Settings .

WebReports Uninstallation

To uninstall WebReports, you use the Windows Add Remove Program tool. The Windows Add Remove Program tool permanently removes the Building Operation product from the computer or server.

有关更多信息,请参阅 WebReports Uninstall .

  • WebReports Overview
  • WebReports Installer and WebReports Components
  • Reports Server Configuration
  • WebReports Installation WorkFlow
  • Windows Roles and Features
  • SQL Server
  • SQL Server Installation Settings
  • WebReports Uninstall