earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: WebReports
功能: 报告
产品版本: 1.8, 1.9
2016/3/17

WebReports Installation WorkFlow

The WebReports installation workflow provides a guide to overall WebReports installation.

The flowchart describes the basic steps in the correct order required for a successful installation of WebReports. Each step in the flowchart is covered under a sub-heading in this topic or described by way of the related links below.

 
action_zoom_plus_stroke Webreports overall installation flowchart
图: Webreports overall installation flowchart
Check installation requirements

Details of the hardware and software requirements of the Reports Server are contained in the Reports Server specification sheet. 有关更多信息,请参阅 报表服务器 .

Configure Windows Roles and Features

Using the Server Manager in Windows Server 2008 R2, Windows Server 2012, or Windows Server 2012 R2, add the IIS server role, select the role services, install .NET Framework 3.5, and .NET Framework 4.5 features.

For Windows Server 2008, add the IIS server role, select the role services, and then add the .NET Framework 3.5.1 features.

有关更多信息,请参阅 Windows Roles and Features .

Install SQL Server

Download SQL Server and then configure the installation settings for WebReports.

有关更多信息,请参阅 SQL Server Installation Settings .

Install WebReports

Install WebReports on the same computer where you installed SQL Server.

有关更多信息,请参阅 Installing WebReports .

  • WebReports Overview
  • WebReports Installation Overview
  • 报表服务器
  • Windows Roles and Features
  • SQL Server Installation Settings
  • Installing WebReports
  • Detaching a WebReports Database
  • Attaching a WebReports Database