The WebReports installation workflow provides a guide to overall WebReports installation.
The flowchart describes the basic steps in the correct order required for a successful installation of WebReports. Each step in the flowchart is covered under a sub-heading in this topic or described by way of the related links below.
Details of the hardware and software requirements of the Reports Server are contained in the Reports Server specification sheet. Pour plus d'informations, voir Reports Server .
Using the Server Manager in Windows Server 2008 R2, Windows Server 2012, Windows Server 2012 R2, or Windows Server 2016, add the IIS server role, select the role services, install .NET Framework 3.5, and .NET Framework 4.x features.
For Windows Server 2008, add the IIS server role, select the role services, and then add the .NET Framework 3.5.1 features.
Pour plus d'informations, voir Windows Roles and Features .
Download SQL Server and then configure the installation settings for WebReports.
Pour plus d'informations, voir SQL Server Installation Settings .
Install WebReports on the same computer where you installed SQL Server.
Pour plus d'informations, voir Installing WebReports .