earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos WebReports
Funcionalidades: Informes
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
16/12/2021

Energy Unit Configuration Errors

When you run one of the three different types of energy reports, it is possible that the report contains an error message informing you that energy units are not configured correctly. For example, you configured a power unit (W) instead of an energy unit (Wh), or you did not assign any unit at all. In these circumstances you need to know which extended trend log is incorrectly configured, and you can find out by clicking directly on the error message link. The subsequent report contains details of relevant trend logs and of the associated energy meter.

For example, you run a Consumption report on Electricity Meter 1 and you see the Units are not configured correctly message:

 
action_zoom_plus_stroke Units are not configured correctly message
Figura: Units are not configured correctly message

If you click on the error message link, a Unit Configuration Errors report is generated (in this example, units have not been configured):

 
action_zoom_plus_stroke Location of extended trend log configuration error
Figura: Location of extended trend log configuration error

You can also generate a Unit Configuration Errors report from the WebReports Diagnostics folder. Para obtener más información, consulte Unit Configuration Errors Report .

You can configure the extended trend log to correct the energy units error. Para obtener más información, consulte Configuración de registro de tendencias ampliado .

  • Configuración de registro de tendencias ampliado
  • Unit Configuration Errors Report
  • WebReports Diagnostic Reports
  • Energy Monitoring Reports