Produkty: WebStation
Funkcje: Trendy
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2021-07-22

Trend Chart Settings Dialog Box – Series Tab

Use the Series tab to change the settings and attach a calculation method to a trend chart series.

 
action_zoom_plus_stroke Series tab
Rysunek: Series tab

Tabela: Series Tab

Component

Description

Color 

Select a color for the series. Więcej informacji zawiera Changing the Color of a Trend Chart Series .

Series presentation  

Select a presentation type for the series. The series can be presented with a line, a discrete line, digital, or bars. Więcej informacji zawiera Trend Series .

Y-axis

Select to display the y-axis to the left or to the right.

Weight

Select the weight of the series.

Show markers

Select True to show a marker for each record. The marker can only be shown for lines and discrete lines, not for digital and bars.

Show events

Select True to show events.

Calculation method

Select the calculation method to calculate the recorded values before displaying the series in the trend chart. Więcej informacji zawiera Calculation Methods .

Delta over period

Select to apply a period to the delta calculation method. Więcej informacji zawiera Calculation Methods .

Period

Select the time span for which the calculation method is to be executed.

Custom period

When Custom period is selected, enter a custom time span for which the calculation method is to be executed.

Custom period alignment 

When Custom period alignment  is selected, enter the time when you want the custom period to start.

  • Trend Chart Series in WebStation
  • Trend Series
  • Changing the Color of a Trend Chart Series
  • Calculation Methods
  • Trend Chart Series Menu
  • Trend Chart Settings Dialog Box – X Axis Tab
  • Trend Chart Settings Dialog Box – Left Axis Tab