earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
5
Concept

Concept


Products: AD v2, AD v1, Technician Tool for Android, Technician Tool for iOS
Functionalities: Basic Functionality, Schedules, Trends
Product version: 1.8, 1.9
2/13/2020

Custom View

arrow1_rotationTrend Logs arrow1_rotationSchedules arrow1_rotationGraphics

Custom View lists the objects and functions that are available in the Custom View folder of Building Operation in a logical manner, such as hierarchical, geographical, or functional. So, you do not see the entire tree structure of WorkStation, just the parts that you want to see or all the parts in the order that you want. For example, in WorkStation, you create a Custom View that contains variables of a Campus that you want to monitor from Technician Tool.

To have Custom View on Technician Tool, an engineer needs to create the Custom View folder in WorkStation consisting of the functions and objects in the order that you want. You can then view and navigate through the system objects using Custom View on Technician Tool. For more information, see Creating Custom View Folder in WorkStation .

The values of the grayed out variables without the Force option are read-only values that you can not change.

The values of the grayed out variables with the Force option can be changed when you force ON . For more information, see Forcing a Value .

A warning icon next to a variable means that the value cannot be converted and may not represent what you are expecting to see. For example, the power consumption variable cannot have units in g/m 2 . The unit should be kWh. This error is represented by warning icon.

The value is displayed in blue font when the value is not older than 3 minutes and there is no network failure.

Using the built-in swipe-to-refresh feature, values and objects can be easily refreshed in Custom View as well as within a particular folder in Custom View .

You can scroll through the long list of objects and variables in Custom View as well as within a particular folder in Custom View using quick scroll bar.

Objects and variables are listed in the same order as in WorkStation.

Note:

Objects and variables listed in Custom View vary according to the software permissions assigned to the user who has logged into Technician Tool. For more information, see User Account Profile Workflow .

 
action_zoom_plus_stroke Custom View in iOS and Android
Figure: Custom View in iOS and Android

Trend Logs

You can view a list of trend logs and their properties. You can filter the trend logs based on date and time as well as search logs based on value. You can view the name, type, and source of trend log.

For more information, see Viewing Trend Logs .

 
action_zoom_plus_stroke TrendLogs for iOS and Android
Figure: TrendLogs for iOS and Android

Schedules

You can view a list of schedules and manage a schedule. Schedule operations are the same as in WebStation.

Schedules are used to schedule the operation of part of the building management system, such as a fan, a door, or a setpoint. Using a schedule, a fan can be set to operate between 08:00 and 17:00 every workday.

Schedules can be overridden by different types of exceptions. For example, if you want to shut the fan down the last Friday in every month due to maintenance, you can use a calculated exception. The exception is added to the schedule and turns off the fan the last Friday in every month.

If you want to shut down the fan during the summer vacation, you can use a Calendar exception. In this case, you use an already created calendar that defines the summer vacation. This calendar is added to the schedule as an exception and the fan will be shut down during all days of the summer vacation defined by the calendar.

You can view schedule details only in landscape mode.

For more information, see Viewing Schedules .

 
action_zoom_plus_stroke Schedules for iOS and Android
Figure: Schedules for iOS and Android

Graphics

You use graphics to display building overviews, display values from sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.

You can view graphics only in landscape mode and also refresh the graphics.

Note:

Panel objects are not supported in Graphics.

 
action_zoom_plus_stroke Graphics in iOS
Figure: Graphics in iOS
 
action_zoom_plus_stroke Graphics in Android
Figure: Graphics in Android
  • Views
  • User Account Profile Workflow
  • Creating Custom View Folder in WorkStation
  • Forcing a Value
  • Editing a Value for an Event
  • Viewing Trend Logs
  • Viewing Schedules