earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AD v2, AD v1, Technician Tool for Android, Technician Tool for iOS
Functionalities: Basic Functionality
Product version: 1.8, 1.9
5/14/2018

Views

arrow1_rotationCustom View arrow1_rotationSystem

In Technician Tool, you can display the Building Operation database in two ways:

  • Custom view: Displays only the objects and folders that you want to see in the order that you want.

  • System view: Displays the entire tree structure of Building Operation as it appears in WorkStation.

You can view the following objects in Technician Tool:

  • Automation Servers (seen only in System view)

  • Alarms

  • Trends

  • Schedules

  • Graphics

  • Function Block Programs

  • Script Programs

  • Devices

Custom View

Custom View lists the objects and functions that are available in the Custom View folder of Building Operation in a logical manner, such as hierarchical, geographical, or functional. So, you do not see the entire tree structure of WorkStation, just the parts that you want to see or all the parts in the order that you want. For example, in WorkStation, you create a Custom View that contains variables of a Campus that you want to monitor from Technician Tool.

For more information, see Custom View .

System

System displays the entire tree structure of Building Operation as it appears in WorkStation.

For more information, see System .

  • Technician Tool Overview
  • System
  • Custom View