Use the Graphic View of the Advanced Schedule editor to edit the properties of an exception or weekly event.
Select a schedule in the System Tree pane.
In the Schedule Editor, click the Advanced tab.
In the Schedule Event Tree, choose one of the following tasks:
To modify an exception, expand the Exceptions folder and Priority x folder. Then, select an exception.
To modify a day, expand the Weekly folder and select a day.
Click the Graphic View button
Right-click on the time period that you want to modify and click Properties .
Edit the properties.
|
Component |
Description |
|
Value |
Enter the value associated with the event. |
|
Start Time |
Click the up or down arrows to select the hours, minutes, and seconds for the start time. You can also type the time if you want. |
|
End Time |
Click the up or down arrows to select the hours, minutes, and seconds for the end time. You can also type the time if you want. |
|
No End Time |
Click the checkbox to have the event last all day. |
Click OK .
On the File menu, click Save .