earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Server, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 1.8
10/14/2016

Add/Remove Columns Dialog Box (Events)

Use the Add/Remove columns dialog box to add or remove columns from the Events pane or an Event View.

 
action_zoom_plus_stroke Add/Remove Columns dialog box
Figure: Add/Remove Columns dialog box

Table: Add/Remove Columns

Component

Description

Acknowledge time

Select to display the time and date when the alarm was acknowledged. For more information, see Acknowledgements .

Alarm state

Select to display the alarm state. For more information, see Alarm States .

Alarm text

Select to display the alarm message that was added to the alarm. For more information, see Alarm Messages .

Assigned state

Select to display the assigned state the alarm had. For more information, see Alarm Assignments .

Assigned to domain

Select to display the domain of the user or group that an alarm was assigned to. For more information, see Domains .

Assigned to ID

​Select to display the ID of the user or group that an alarm was assigned to.

Assigned to name

Select to display the name of the user or group that an alarm was assigned to. For more information, see Alarm Functions .

BACnet alarm type

Select to display the BACnet alarm that monitored a variable within a BACnet network.

Basic evaluation state

Select to display the basic evaluation state of an alarm. The value True indicates that an alarm was triggered.

Category

Select to display the alarm category name.

Command

Select to display the executed command.

Comment

Select to display the comment that was added to an alarm.

Control Source

Select to display the initials of the controlling I/NET operator.

Control State

Select to display the 4 bit I/NET state descriptor.

Count

Select to display the number of times an alarm has toggled between the alarm and reset state. For more information, see Count .

Description

Select to display the event description. For more information, see General Information Properties – Basic Tab .

Device Name

Select to display the name of the I/NET device that generated the event.

Disabled cause

Select to display the cause for why the alarm was disabled. An alarm can be disabled by user, shunt variable and/or system (it’s disabled by system if the alarm was incorrectly configured).

Domain name

Select to display the domain a user belonged to. For more information, see Domains .

Evaluation State

Select to display the evaluation state an alarm had. For example, Upper limit alarm is displayed if the monitored value reached the upper alarm limit.

EWS ID

Select to display the EcoStruxure Web Service identification of the event on the external system.

EWS source ID

Select to display the EcoStruxure Web Service identification of the external object that generated the event.

EWS source name

Select to display the events ty the name of the external object that generated the event.

First Name

Select to display the first name of the individual whose key/card was used at the I/NET door point.

Forced value

Select to display the forced values.

Group

Select to display the name of the cause note or action note group the user edited.

Hidden

Select to display the visible status an object had. False is displayed when an object was shown.

Individual

Select to display the individual number of the individual whose key/card was used at the I/NET door point.

INET Address

Select to display the system address of the point, or station address of the host or controller that generated the event.

INET Event Type

Select to display the I/NET event type.

Last Name

Select to display the last name of the individual whose key/card was used at the I/NET door point.

LinkName

Select to display the name assigned to the link of the device from which the event originated.

Message Text

Select to display the text of an I/NET action or dispatch message, if there is one.

Monitored variable

Select to display the path of the monitored variable.

Note

Select to display event notes.

Previous alarm state

Select to display the previous alarm state.

Priority

Select to display the​ priority an alarm had.

Sequence number

Select to display the event sequence number on the present server.

Sigma event parameters

Select to display parameters of the Sigma event.

Sigma event type

Select to display the Sigma event type.

Source

Select to display the path of the source object.

Source server

Select to display the server path of the source object.

State

Select to display the events in (up to) 4 text characters that represent the text state of a discrete point or the unit description of an analog point.

StationName

Select to display the name assigned to the device from which the event originated.

System alarm ID

Select to display the alarm ID generated by the system.

System event ID

Select to display the event ID generated by the system.

Tenant

Select to display the tenant number of the individual whose key/card was used at the I/NET door point.

Text

Select to display the text messages in the E-mail in a E-mail notification. For more information, see Notifications .

Timestamp

Select to display the time and date when the event was generated.

Triggered time

Select to filter events by the time and date an alarm went from normal state to alarm state.

Type

Select to display the event type. For more information, see General Information Properties – Basic Tab .

Unique alarm ID

Select to display the ID of the alarm that generated the event.

Unique user ID

Select to display the ID of the user that generated the event.

User action item

Select to display events of which the user has edited checklist, cause note group, or action note group items.

User name

Select to display the name of the user that generated the event.. For more information, see Events Pane and Event View Customization .

Value after

Select to display the value of an object after it was changed.

Value at change

Select to display the value the monitored variable had when the alarm was triggered.

Value before

Select to display the value of an object before it was changed.

Zone

Select to display the I/NET security zone number associated with a security event (0-63).

  • Events Pane and Event View Customization
  • Add/Remove Columns Dialog Box
  • Quick Filter
  • Filter Condition Wildcards