Use the Add/Remove Columns dialog box to add or remove columns from the Alarms pane or an Alarm View.
Component |
Description |
Acknowledge time |
Select to display the time and date when the alarm was acknowledged. For more information, see Alarm Acknowledgements . |
Acknowledged by |
Select to display the name of the individual who acknowledged the alarm. For more information, see Alarm Acknowledgements . |
Acknowledgement required |
Select to display the required acknowledgement to acknowledge the alarm. For more information, see Alarm Acknowledgements . |
Alarm state |
Select to display the state of the alarm. For more information, see Alarm States . |
Alarm text |
Select to display the alarm message that is added to the alarm. For more information, see Alarm Messages . |
Assigned state |
Select to display the assigned state of the alarm. For more information, see Alarm Assignments . |
Assigned to domain |
Select to display the domain of the user or user group that an alarm is assigned to. For more information, see Domains . |
Assigned to ID |
Select to display the ID of the user or group that an alarm was assigned to. |
Assigned to name |
Select to display the name of the user or user group that an alarm has been assigned to. |
BACnet alarm type |
Select to display the BACnet alarm type of the alarm that monitored a variable within a BACnet network. |
BACnet notification |
Select to display the distribution information of an alarm notification within a BACnet system |
BACnet notification type |
Select to display the distribution information type of an alarm notification within a BACnet system.. |
Basic evaluation state |
Select to display the basic evaluation state of an alarm. The value True indicates that an alarm is triggered. |
Category |
Select to display the alarm category name. |
Command value |
Select to display the value that was commanded. |
Confirmed notification |
Select to display whether or not the Building Operation server that received transmission of data has sent a confirmation to the sending device that the data has been received. |
Count |
Select to display the number of times an alarm has toggled between the alarm and reset state. For more information, see Count . |
Deadband |
Select to display the deadband value of the alarm. |
Device name |
Select to display the name of the I/NET device that generated the alarm. |
Disabled by |
Select to display the name of the user who disabled the alarm. |
Disabled cause |
Select to display the cause for disabling the alarm. An alarms can be disabled by a user, a shunt variable, or, if incorrectly configured, by the system. |
Error limit |
Select to display the difference limit that was exceeded. |
Evaluation state |
Select to display the evaluation state of an alarm. For example, Upper limit alarm is displayed if the monitored variable reached the upper alarm limit. |
Event from state |
Select to display the event state after the occurrence that initiated the notification. |
EWS ID |
Select to display the EcoStruxure Web Service identification of the alarm in the external system. |
EWS source ID |
Select to display the EcoStruxure Web Service identification of the external object that generated the alarm. |
Exceeded limit |
Select to display the limit that was exceeded. |
Exceeding value |
Select to display the value that exceeded the limit. |
Feedback value |
Select to display the value that differs from the Command value. |
First name |
Select to display the first name of the individual whose key/card was used at the I/NET door point. |
Hidden |
Select to display the visible status of an object. False is displayed when an object is shown. |
Individual |
Select to display the individual number of the individual whose key/card was used at the I/NET door point. |
Last name |
Select to display the last name of the individual whose key/card was used at the I/NET door point. |
Logging |
Select to display whether or not associated alarm events are generated and recorded in the event log. |
Message text |
Select to display the text of an I/NET action or dispatch message, if there is one. |
Monitored variable |
Select to display the path of the monitored variable. |
New mode |
Select to display the new mode of the referenced object. |
New state |
Select to display the new state of the referenced object. |
New value |
Select to display the new value of the referenced property. |
Operation expected |
Select to display the next operation requested by the referenced object. |
Possible operator actions |
Select to display the actions available to the operator. |
Previous alarm state |
Select to display the previous alarm state of an alarm. |
Priority |
Select to display the priority of an alarm. |
Process ID |
Not used. |
Reference bit string |
Select to display the new value of the referenced bitstring property. |
Sequence number |
Select to display the alarm sequence number on the present Building Operation server. |
Setpoint value |
Select to display the value of the reference variable. |
Sigma event parameters |
Select to display parameters of the Sigma event that generated the alarm. |
Sigma event type |
Select to display the type of Sigma event that generated the alarm. |
Source |
Select to display path of the source object. |
Source name |
Select to display the name of the source object. |
Source server |
Select to display the server path of the source object. |
Status flags |
Select to display the status flag of the object. |
System alarm ID |
Select to display the alarm ID generated by the system. |
Tenant |
Select to display tenant number of the individual whose key/card was used at the I/NET door point. |
Timestamp |
Select to display the time and date when the alarm was generated. |
Triggered time |
Select to filter alarms by the time and date the alarm went from normal state to alarm state. |
Type |
Select to display the alarm type. For more information, see General Information Properties – Basic Tab . |
Value at change |
Select to display the value the monitored variable had when the alarm was triggered. |