earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Alarms, Basic Functionality
Product version: 2023
9/20/2024

Add/Remove Columns Dialog Box (Alarms)

Use the Add/Remove Columns dialog box to add or remove columns from the Alarms pane or an Alarm View.

 
action_zoom_plus_stroke Add/Remove Columns dialog box
Figure: Add/Remove Columns dialog box

Table: Add/Remove Columns Dialog Box

Component

Description

Acknowledge time

Select to display the time and date when the alarm was acknowledged. For more information, see Alarm Acknowledgements .

Acknowledged by

Select to display the name of the individual who acknowledged the alarm. For more information, see Alarm Acknowledgements .

Acknowledgement required

Select to display the required acknowledgement to acknowledge the alarm. For more information, see Alarm Acknowledgements .

Alarm state

Select to display the state of the alarm. For more information, see Alarm States .

Alarm text

Select to display the alarm message that is added to the alarm. For more information, see Alarm Messages .

Assigned state

Select to display the assigned state of the alarm. For more information, see Alarm Assignments .

Assigned to domain

Select to display the domain of the user or user group that an alarm is assigned to. For more information, see Domains .

Assigned to ID

​Select to display the ID of the user or group that an alarm was assigned to.

Assigned to name

Select to display the name of the user or user group that an alarm has been assigned to.

BACnet alarm type

Select to display the BACnet alarm type of the alarm that monitored a variable within a BACnet network.

BACnet notification

Select to display the distribution information of an alarm notification within a BACnet system

BACnet notification type

Select to display the distribution information type of an alarm notification within a BACnet system..

Basic evaluation state

Select to display the basic evaluation state of an alarm. The value True indicates that an alarm is triggered.

Category

Select to display the alarm category name.

Command value

Select to display the value that was commanded.

Confirmed notification

Select to display whether or not the EcoStruxure BMS server that received transmission of data has sent a confirmation to the sending device that the data has been received.

Count

Select to display the number of times an alarm has toggled between the alarm and reset state. For more information, see Count .

Custom Audio

Select to display the Custom Audio file for the alarm.

Deadband

Select to display the deadband value of the alarm.

Device name

Select to display the name of the I/NET device that generated the alarm.

Disabled by

Select to display the name of the user who disabled the alarm.

Disabled cause

Select to display the cause for disabling the alarm. An alarms can be disabled by a user, a shunt variable, or, if incorrectly configured, by the system.

Dispatch message

Select to display the Dispatch message text assigned to the I/NET alarm

Error limit

Select to display the difference limit that was exceeded.

Evaluation state

Select to display the evaluation state of an alarm. For example, Upper limit alarm is displayed if the monitored variable reached the upper alarm limit.

Event from state

Select to display the event state after the occurrence that initiated the notification.

EWS ID

Select to display the EcoStruxure Web Service identification of the alarm in the external system.

EWS source ID

Select to display the EcoStruxure Web Service identification of the external object that generated the alarm.

Exceeded limit

Select to display the limit that was exceeded.

Exceeding value

Select to display the value that exceeded the limit.

Feedback value

Select to display the value that differs from the Command value.

Fire zone

Select to display the number of the zone from which the alarm originates. Displays 0 if no zone is configured.

First name

Select to display the first name of the individual whose key/card was used at the I/NET door point.

Hidden

Select to display the visible status of an object. False is displayed when an object is shown.

Individual

Select to display the individual number of the individual whose key/card was used at the I/NET door point.

Last comment

Select to display the last comment on a triggered alarm.

Last name

Select to display the last name of the individual whose key/card was used at the I/NET door point.

Logging

Select to display whether or not associated alarm events are generated and recorded in the event log.

Message text

Select to display the text of an I/NET action or dispatch message, if there is one.

Monitored variable

Select to display the path of the monitored variable.

New mode

Select to display the new mode of the referenced object.

New state

Select to display the new state of the referenced object.

New value

Select to display the new value of the referenced property.

Operation expected

Select to display the next operation requested by the referenced object.

Possible operator actions

Select to display the actions available to the operator.

Previous alarm state

Select to display the previous alarm state of an alarm.

Priority

Select to display the priority of an alarm.

Process ID

Not used.

Reference bit string

Select to display the new value of the referenced bitstring property.

Sequence number

Select to display the alarm sequence number on the present EcoStruxure BMS server.

Setpoint value

Select to display the value of the reference variable.

Sigma event parameters

Select to display parameters of the Sigma event that generated the alarm.

Sigma event type

Select to display the type of Sigma event that generated the alarm.

Source

Select to display path of the source object.

Source name

Select to display the name of the source object.

Source server

Select to display the server path of the source object.

Status flags

Select to display the status flag of the object.

System alarm category

Select to display the category of a fire detection system alarm.

System alarm ID

Select to display the alarm ID generated by the system.

Tenant

Select to display tenant number of the individual whose key/card was used at the I/NET door point.

Timestamp

Select to display the time and date when the alarm was generated.

Triggered time

Select to filter alarms by the time and date the alarm went from normal state to alarm state.

Type

Select to display the alarm type. For more information, see General Information Properties – Basic Tab .

Value at change

Select to display the value the monitored variable had when the alarm was triggered.

  • Alarms Pane and Alarm View Customization
  • Add/Remove Columns Dialog Box
  • Quick Filter
  • Filter Condition Wildcards