earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: AS-C, AS-B, Enterprise Server, Function Block Editor, Graphics Editor, AS-P, Project Configuration Server, Project Configuration Tool, WebReports, Script Editor, SmartXKiosk
Funzionalità: Programmazione, Ingegneria, Grafica, Importazione/esportazione, Report
Versione del prodotto: 1.8
13/10/2016

Engineering Tools Overview

You engineer your system using the engineering tools.

Spreadsheet Overview

You use the Spreadsheet view to create and edit multiple objects and to save time.

Per maggior informazioni, consulta Spreadsheet Overview .

Bindings Overview

A binding is a connection between two or more variables for data exchange. In its simplest form, a binding consists of a source and a destination. The source supplies the value to the destination.

Per maggior informazioni, consulta Bindings Overview .

Text Reports Overview

A text report provides a simple and quick method of obtaining a customized view of object property attributes.

Per maggior informazioni, consulta Text Reports Overview .

Import and Export Overview

A solution or application is a user-created object or group of objects that perform a control process. Examples of creatable objects in Building Operation include networks, devices, programs, binding templates, graphics, trends, and alarms.

Per maggior informazioni, consulta Import and Export Overview .

Script Overview

Script programs are text-based instructions that tell the SmartStruxure server to take some kind of action to control a building.

Per maggior informazioni, consulta Script Overview .

Function Block Editor Overview

Function Block Editor is a graphical programming tool for SmartStruxure server devices, which you use to create function block programs that control and monitor building automation systems. For example, you create a basic program, called OfficeLight, to control lighting in a room based on occupancy.

Per maggior informazioni, consulta Function Block Editor Overview .

Graphics Editor Overview

​You can use Graphics Editor to create and edit graphics representing a site and the devices that make up the site.

Per maggior informazioni, consulta Graphics Editor .

WebReports Overview

​WebReports is a Web application that you use to create, view, and administer reports. The reports provide information about alarms, trends, and user and system activity. You use the reports to help manage your building automation system.

Per maggior informazioni, consulta WebReports Overview .

WorkStation for Projects Overview

Project Configuration Server with WorkStation for Projects is an offline engineering platform that is used for project configuration and deployment.

A dedicated engineering platform separate from the target system facilitates flexibility. You do not need to spend as much time at the customer site. Much of the analyzing, designing, modelling, and programming can be done at your office at your convenience, in a similar way as in WorkStation.

Per maggior informazioni, consulta WorkStation for Projects Overview .

Vista Conversion Overview

To assess whether or not to convert a Vista system to Building Operation, you run an analysis of the Vista database export file to get information on the potential outcome of a conversion. The analysis is performed on Transition Portal. If the analysis confirms that the Vista database is suitable for conversion, you can convert the database in TAC Vista to SBO Conversion Tool.

Per maggior informazioni, consulta Vista Conversion Overview .

Continuum Conversion Overview

Conversion is the process by which a customer's site is moved from Andover Continuum's legacy Building Management System to StruxureWare Building Operation. The Andover Continuum to StruxureWare Building Operation (SBO) Conversion Tool takes an ASCII dump from the Continuum system and creates SBO objects that correspond to the objects in the ASCII dump file.

Per maggior informazioni, consulta Continuum Conversion Overview .

SmartXKiosk Overview

The SmartXKiosk app allows you to configure AD as a dedicated HMI for local access to SmartStruxure servers.

Per maggior informazioni, consulta SmartXKiosk Overview .

SmartX AD-Link Overview

The SmartX AD-Link app allows you to use a USB connection for TCP/IP network communication between AD and a SmartStruxure server.

Per maggior informazioni, consulta SmartX AD-Link Overview .

  • Building Operation Overview
  • Spreadsheet Overview
  • Bindings Overview
  • Text Reports Overview
  • Import and Export Overview
  • Script Overview
  • Function Block Editor Overview
  • Graphics Editor
  • WebReports Overview
  • WorkStation for Projects Overview
  • Vista Conversion Overview
  • Continuum Conversion Overview
  • SmartXKiosk Overview
  • SmartX AD-Link Overview