earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 3.0, 3.1
5/13/2019

EcoStruxure Building Management Overview

EcoStruxure Building Management is an integration platform for monitoring, control, and management of energy, lighting, fire safety, security and HVAC.

Work Interface Overview

You use interfaces to set up, manage and operate the EcoStruxure BMS on a daily basis.

For more information, see Work Interface Overview .

EcoStruxure BMS Server Overview

EcoStruxure BMS servers are used to engineer and supervise Building Management Systems.

For more information, see EcoStruxure BMS Server Overview .

Function Overview

The EcoStruxure Building Operation software gives you a number of functions to monitor and manage your facilities.

For more information, see Function Overview .

Engineering Tools Overview

You engineer your system using the engineering tools.

For more information, see Engineering Tools Overview .

Protocol Overview

The EcoStruxure Building Operation software supports the major communication protocols in building automation and security management.

For more information, see Protocols Overview .

Hardware Overview

The Schneider Electric hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, I/O modules, SmartX servers such as SmartX AS-P servers and SmartX AS-B servers, SmartX IP Controller devices such as MP-Cs, MP-Vs, IP-IO modules, and RP-Cs, SmartX Sensors, and ADs.

For more information, see Hardware Overview .

Licensing, Installation, and Localization Overview

To be able to run the EcoStruxure Building Operation software you need to install and licensing the software.

For more information, see Licensing, Installation, and Localization Overview .

System Registration Overview

Registering your EcoStruxure Building Operation software ensures that you get better services, warranty, and critical system information.

For more information, see System Registration .

System Upgrade Overview

A system upgrade can include an Enterprise Server, Reports Server, one or more SmartX servers and WorkStations, and the supporting administrator software, such as Device Administrator.

For more information, see System Upgrade Overview .

  • Work Interface Overview
  • EcoStruxure BMS Server Overview
  • Function Overview
  • Engineering Tools Overview
  • Protocols Overview
  • Hardware Overview
  • Licensing, Installation, and Localization Overview
  • System Registration
  • System Upgrade Overview