earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Device Administrator, Enterprise Central, Enterprise Server, Function Block Editor, Graphics Editor, ​License Administrator, ​License Server, AS-P, Script Editor, Software Administrator
Functionalities: Basic Functionality, License Management, Localization
Product version: 2.0, 2.1, 3.0, 3.1
5/18/2018

Licensing, Installation, and Localization Overview

To be able to run the EcoStruxure Building Operation software you need to install and licensing the software.

Licensing Overview

The EcoStruxure Building Operation software is available for all to download and install. However, you need valid licenses to use the software. The number of users of the software is limited to the number of licenses owned by the customer.

For more information, see Licensing Overview .

Installation Overview

The EcoStruxure Building Operation software products are installed using installation packages.

For more information, see Installation Overview .

Regional and Language Overview

WorkStation presents language, date, time, currency, unit, and decimals according to the user’s operating system settings.

For more information, see Regional and Language Overview .

  • EcoStruxure Building Management Overview
  • Licensing Overview
  • Installation Overview
  • Regional and Language Overview