earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WorkStation
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 2024, 7.0
2024-12-09

Searching for Forced Values

You search for forced values to determine if the system runs normally and to reset forced values. Manually overridden I/O points are not included in the search result.

Visa mer
action_close

When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.

You can manually release a forced value at any time or you can automate the release, using a Timed Force utility object to specify the duration or end time of the force. Mer information finns i Timed Force Objects .

When you release a forced value, the value returns to its normal status.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. Mer information finns i Viewing an Unforced Value .

Timeout on forced values

You can set a timeout on forced values so that the forced value is automatically unforced after a fixed time. The time can be a duration, for example two hours. The forced value can also be unforced at a specific calendar date and time.

Mer information finns i Setting a Timeout on a Forced Value .

Mer information finns i Setting a Timeout on a Forced Value WebStation .

Indication in WorkStation

A forced value is indicated by orange color in the properties dialog boxes. In in the Watch pane, a forced value is indicated by a pointing hand

 
action_zoom_plus_stroke
.

In the List View and Search View, a forced value is indicated by the text [Forced] in the 'Value' column.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. Mer information finns i Viewing an Unforced Value .

Indication in WebStation

A forced value is indicated by orange color and a pointing hand in the List view.

Indication in Function Block Graphics Viewer

A forced value is indicated by orange color in Function Block Graphics Viewer. Mer information finns i Forced Value Indication in Function Block Graphics Viewer .

Search for forced values

You can search for forced values using the search function in WorkStation.

Mer information finns i Searching for Forced Values .

You can search for forced values in WebStation using Diagnostics.

Mer information finns i Displaying a List of Forced Values in WebStation .

To search for forced values
  1. In WorkStation, on the Toolbar, click the Search button

     
    action_zoom_plus_stroke
    .

  2. In the Search view, in the text box, type your search.

    Obs!

    To search for all forced values, type '*'.

  3. In the In folder box, enter the folder where you want to start the search.

  4. Select Include subservers to include field subservers in the search.

    Obs!

    Only subservers running EcoStruxure Building Operation BMS version 1.5 or higher are included in the search.

  5. Select Stop if more than 1000 results to limit the search to 1,000 results.

  6. Select Forced values only to search for forced values that were forced from within the EcoStruxure BMS.

  7. Select In device to include values forced from outside the EcoStruxure BMS in the search. For example, values forced on the device.

  8. In the Select Types dialog box, in the Include types box, select object types to include in your search.

  9. Click the Add type button

     
    action_zoom_plus_stroke
    .

  10. Click OK .

  11. In the Select Conditions box, enter the search conditions that have to be met before a search result is displayed.

  12. Click the Add condition button

     
    action_zoom_plus_stroke
    and select the condition you want to use for the search.

  13. Click OK .

  14. Click the Search button

     
    action_zoom_plus_stroke
    .

The forced values in the EcoStruxure BMS are displayed.

  • Search
  • Search Overview
  • Forced Values
  • Search View
  • Search View Toolbar