earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AO-8, AO-V-8, AS-L, DI-16, DO-FA-12, DO-FC-8, AS-P, PS-24 V, RTD-DI-16, UI-16, UI-8/AO-4, UI-8/AO-V-4, UI-8/DO-FC-4
Funcionalidades: Hardware
Versión del producto: 2.0, 2.1, 3.0, 3.1
07/06/2020

Electronics Modules

The electronics module is the main component of Smart devices that are based on the patented two-piece design. The electronics module is installed on a terminal base, which constitutes the second component of the device.

The electronics module has two handles, which have to be pulled out when removing the module from or inserting the module to the terminal base. In their inner position, the handles lock the module to the terminal base. This effectively helps prevent unintentional separation. Two plastic label carriers can carry labels that show field markings. Wiring connections are made at terminal blocks contained on the terminal base. The terminal screws are accessible without removing the module. Power for all devices is taken from the 24 VDC rails of the backplane that is part of the terminal base.

 
action_zoom_plus_stroke ​General assembly
Figura: ​General assembly

Number

Device Parts

 
action_zoom_plus_stroke

Electronics module

 
action_zoom_plus_stroke

Terminal block

 
action_zoom_plus_stroke

Terminal base

 
action_zoom_plus_stroke

Ventilation slot

 
action_zoom_plus_stroke

Label carrier

 
action_zoom_plus_stroke

DIN rail

 
action_zoom_plus_stroke

Backplane board with device label

 
action_zoom_plus_stroke

LEDs

 
action_zoom_plus_stroke

Handle

  • Hardware Overview
  • PS-24V Power Supplies
  • Automation Servers
  • SmartX AS-P Servers
  • I/O Modules
  • Terminal Bases
  • Installing an Electronics Module on a Terminal Base
  • Powering Up a Device
  • Printing a Label to Identify I/O Channels