LED Patterns |
Condition/Mode |
Blue, flashing (2 s ON, 8 s OFF) |
Default Mode (No Bluetooth client connection, no SmartX IP controller connection) |
Blue, flashing (1 s ON, 1 s OFF) |
Advertising Mode (No Bluetooth client connection, no SmartX IP controller connection, connection is possible) |
Blue, constant (always ON) |
Connected Mode (Bluetooth client connection, no SmartX IP controller connection) |
Blue, ON when transmitting, OFF otherwise |
Active Mode (Bluetooth client connection, SmartX IP controller connection active) |
Blue, flashing (2 s ON, 6 s OFF, 8 s ON, 4 s OFF) |
DFU Mode (Waiting for user to press and hold push-button) |