earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: User Management
5/13/2025

Editing Relative Path Permissions Templates

You modify a relative path permission by adding or withdrawing permissions for this folder structure. The changes will be accounted in all the instance.

Relative path permissions for a folder structure grant a specific set of permissions to a user account group or to a user account to all the folders accessible in a predefined path and its folder structure. Relative path permissions enable a user accounts group or a user account to reuse a specific path permission.

Furthermore, you can add and delete permissions for this folder structure.

Show More
action_close

Relative path permissions for a folder structure grant a specific set of permissions to a user account group or to a user account to all the folders accessible in a predefined path and its folder structure. Relative path permissions enable a user accounts group or a user account to reuse a specific path permission.

Furthermore, you can add and delete permissions for this folder structure.

Example

The same set of objects and properties (values, trends, alarms, graphics etc.) is defined in 100 rooms in your building. You define a relative path template that models the folder structure of the rooms in the building, and you define permissions to this folder structure. You define a relative path template by choosing one example of the folder structure. All similar folder structures following the same pattern will inherit permissions defined on the template. Finally, you also define permissions for specific user accounts and user account groups.

For more information, see Creating Relative Path Templates .

Relative Path Permissions Rules

You set permissions on a relative path twice.

First, you set permissions on the objects in the template. Objects in the template can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

Second, you set permissions for user accounts and user account groups. A user account or a user account group can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

For more information, see Relative Path Permissions Rules .

To edit a relative path permissions template
  1. In Workstation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Relative path permissions .

  4. In the Tree Pane select the relative path permissions you want to edit.

  5. In the permissions column, select permissions that you want to assign and unselect permissions you want to withdraw.

  6. Click the Save button

     
    action_zoom_plus_stroke
    .

You modified permissions that user accounts and user account groups have to a folder structure.

  • Relative Path Permissions
  • Assigning Relative Path Permissions to User Accounts or User Account Groups
  • Creating Relative Path Templates