earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server, ​License Administrator, ​License Server, WorkStation, WebStation
Functionalities: Basic Functionality, License Management
7/1/2025

Software and Features that Require Licenses

There are a number of different clients, servers, and features that requires licenses to operate.

EcoStruxure Building Operation

Refer to the document Part Number Summary and Hardware Software Matrix for software and features that need licenses, available on Schneider Electric Extranet.

Information regarding licenses can also be found on the specification sheets:

WorkStation For more information, see WorkStation .

WebStation

AS-P

AS-B

Edge Server

Enterprise Central For more information, see Enterprise Central .

Enterprise Server For more information, see Enterprise Server .

EcoStruxure Fire Operation

Information on which licenses that are available for EcoStruxure Fire Operation are found in the specifications:

WorkStation For more information, see WorkStation .

WebStation For more information, see WebStation .

FDP server For more information, see FDP Server .

Enterprise Central For more information, see Enterprise Central .

Enterprise Server For more information, see Enterprise Server .

  • Licensing Overview
  • License Enforcement