earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: ​License Administrator, ​License Server
Functionalities: License Management
2/27/2025

Licensing Overview

The EcoStruxure Building Operation software is available for all to download and install. However, you need valid licenses to use the software. The number of users of the software is limited to the number of licenses owned by the customer.

Centralized Licensing

Device Administrator is used to manage Centralized Licensing on EcoStruxure BMS servers. Centralized Licensing is the main Licensing feature in EcoStruxure Building Operations.

For more information, see Centralized Licensing Overview .

Licenses Administered by License Administrator

Some licenses needs to be administrated by License Administrator.

For more information, see Licenses Administrated by License Administrator Overview .

Licenses Administrated by License Administrator Components

To install and use licenses, you need three main components:

  • License Activation Server

    for Centralized Licensing and licenses administered by License Administrator.

  • License Server

    for licenses administered by License Administrator.

  • License Administrator

    for licenses administered by License Administrator.

For more information, see Licenses Administrated by License Administrator Components .

Software and Features that Require Licenses

A number of software and features need licenses.

For more information, see Software and Features that Require Licenses .

Demo Licenses

Demo licenses are used for demonstration purposes, training, or when building a site.

For more information, see Demo Licensing Overview .

License Enforcement

License enforcement is the process of checking whether a software application has a valid license available to it at runtime. If you do not have enough licenses, a license violation occurs. This is accomplished by a license violation bar in WorkStation and WebStation.

If a client, such as WorkStation or one of the editors, attempts to start and cannot locate an available license, the client does not start.

For more information, see License Enforcement .

License Information

The License Information in the Control Panel gives you an overview of the licenses in your EcoStruxure BMS.

For more information, see License Information .

Reclaim Licenses

Reclaiming licenses is the process of making sure that the licenses are updated with the latest information.

For more information, see Reclaim Licenses .

  • Licensing, Installation, and Localization Overview
  • Licenses Administrated by License Administrator Components
  • Software and Features that Require Licenses
  • License Information
  • Centralized Licensing Overview
  • Demo Licensing Overview
  • Reclaim Licenses