Fire detection is at the core of an EcoStruxure Building Management System (BMS). The Esmi Sense FDP server provides communication and connectivity to the fire detection system. This field server performs key functionality, such as control logic, trend logging, and alarm supervision, and supports communication and connectivity to the fire detection system. The distributed intelligence of the EcoStruxure BMS helps ensure fault tolerance against detected faults and provides a fully featured user interface through WorkStation and WebStation.
The Esmi Sense FDP server can act as a standalone server to manage the fire detection system or as a native server in the EcoStruxure BMS architecture.
The Esmi Sense FDP server has the following features:
Communications hub
Authentication and permissions through powerful systems
WorkStation/WebStation interface
Native BACnet support
Native OPC UA Client support
Native Modbus support
EcoStruxure Web Services support
MQTT IoT protocol support
External log storage option
Reporting
Scalable configurations
Text and graphics-based programming tools
IT friendly networking based on the TCP/IP suite of communication protocols
TLS support
Capable of coordinating traffic from above and below its location, the Esmi Sense FDP server can deliver data directly to you or to other servers throughout the site. The Esmi Sense FDP server provides access to the full fire detection system and can run multiple control programs, manage alarms, and users, handle scheduling and logging, and communicate using a variety of protocols. Because of this, most parts of the system function autonomously and continue to run as a whole even if communication is interrupted or individual EcoStruxure BMS servers or devices go offline.
An EcoStruxure BMS provides a powerful permission system that is easy to manage, flexible, and adapts to all kinds of system sizes. The permission system provides a high standard of authentication. Authentication is done against the built-in user account management system or against Windows Active Directory Domains. The built-in account management system allows an administrator to establish password policies that meet stringent cybersecurity guidelines. When Windows Active Directory is used, the administration costs are lower because users do not have to be managed in multiple directories.
Through any client, the user experience is similar regardless of which EcoStruxure BMS server the user is logged on to. The user can log directly on to an Esmi Sense FDP server to engineer, commission, supervise, and monitor the Esmi Sense FDP server as well as the fire detection system. See the WorkStation and WebStation specification sheets for additional information.
One of the cornerstones of the EcoStruxure BMS is support for open standards. The Esmi Sense FDP server can natively communicate with some of the most popular standards for buildings: BACnet/IP, OPC UA Client, and Modbus TCP/IP.
The Esmi Sense FDP server communicates directly to BACnet/IP networks. The Esmi Sense FDP servers are BTL-listed as BACnet Building Controllers (B-BC), the most advanced BACnet Device Profile. This capability provides access to an extensive range of BACnet devices from Schneider Electric and other vendors. See the BTL Product Catalog for up-to-date details on BTL listed firmware revisions on BACnet International's home page. An Esmi Sense FDP server can also serve as a BACnet Broadcast Management Device (BBMD) to facilitate BACnet systems that span multiple IP subnets.
OPC UA Client functionality is natively supported in Enterprise Server and field servers, enabling powerful and high-capacity integration of devices or systems that have OPC UA Server capability. OPC Unified Architecture (OPC UA) is a standard originating from industrial automation and process control that provides methods intended to provide improved security, performance, and engineering efficiency. With OPC UA Client support, the EcoStruxure BMS software can monitor and control a wide variety of devices or systems, from Schneider Electric as well as from other companies.
The Enterprise Server and Esmi Sense FDP server natively integrate Modbus TCP/IP client and server configurations. This allows full access to third-party products and the range of Schneider Electric products that communicate on the Modbus protocol, such as power meters, UPS, circuit breakers, lighting controllers, and emergency lighting.
Modbus device types are pre-configured Modbus applications for quick and easy Modbus device integration in EcoStruxure BMS solutions. For information on the Modbus devices supported using Modbus device types, see the document EcoStruxure Building - Modbus Device Integration - Supported Device Brochure.
EcoStruxure Web Services, Schneider Electric’s Web Services standard, is natively supported in the EcoStruxure BMS servers. EcoStruxure Web Services offers extra features between compliant systems whether within Schneider Electric or other authorized systems. These features include system directory browsing, read/write of current values, alarm receipt and acknowledgement, and historical trend log data. EcoStruxure Web Services requires user name and password to log on to the system.
The Enterprise Server and field servers support MQTT as an option for publishing data to, and receiving updates from, other systems. MQTT is a messaging transport protocol that with its small footprint, light bandwidth utilization, and simplicity, is ideal for M2M and IoT communication. The MQTT capability supports communication with any MQTT broker, for example, Amazon, Microsoft, Google or IBM.
EcoStruxure BMS servers can be configured to automatically store all historical data, trend log data, event log and audit trail data, in an external database. If data needs to be available for longer periods of time, an external log storage can be incorporated into the EcoStruxure BMS without the need for extensive engineering work. The supported databases are TimescaleDB, which is built on PostgreSQL, and Microsoft SQL Server. The data in the external log storage is available natively to the viewers built into the EcoStruxure BMS clients and to the built-in reporting functionality.
You can use the powerful Log Processor functionality for custom processing of trend data for viewing in charts, dashboards and for inclusion in reports. The Log Processor enables advanced calculations on one or multiple trend logs and point values.
Examples of advanced calculations:
Energy usage normalization
Virtual submeters and summaries
Calculation of Mean Kinetic Temperature
Unit conversions
Average, maximum, and mini m um over custom periods
The output of the Log Processor can be saved in the database, including the External Log Storage or calculated automatically on demand.
Selected trend logs and the event log can be sent to AVEVA PI System directly without the need for intermediate storage or specialized PI System connectors.
The EcoStruxure BMS servers provide built-in functionality for basic reporting that can deliver reports in any text format and XLSX, without any dependencies to other external software. Reports for XLSX can be enriched by using advanced functionality such as formulas, conditional formatting, charts and sparklines.
Reports can be generated on schedule, on an alarm event or other custom conditions, and you can get the output delivered via email or written to file.
The Esmi Sense FDP server can represent up to 32 Esmi Sense FDP fire detection panels connected in a network and the associated loop devices. The Esmi Sense FDP server can access those fire detection panels that are configured as visible to the Esmi Sense FDP fire panel running the EcoStruxure Fire Operation software. The Esmi Sense FDP server will automatically create all components of the fire detection system based on the active fire detection system configuration that exists in the Esmi Sense FDP server.
Unique to the industry, the EcoStruxure BMS servers have both Script and Function Block programming options. This flexibility helps assure that a suitable programming method can be selected for the application.
The EcoStruxure BMS servers communicate using the networking standards. This makes installations easy, management simple, and transactions more secure.
IP addressing
TCP communications
DHCP for easy network configuration
DNS for simple lookup of addresses
HTTP/HTTPS for Internet access through firewalls, which enables remote monitoring and control
NTP (Network Time Protocol) for time synchronization through the fire detection system configuration
SMTP or SMTPS with support for SSL/TLS based authentication, enables sending email messages triggered by schedule or alarm
Communication between clients and the EcoStruxure BMS servers , and between EcoStruxure BMS servers, can be encrypted using Transport Layer Security (TLS ). The servers are delivered with a default self-signed certificate. Commercial Certification Authority (CA) server certificates are supported to lower the risk of malicious information technology attacks. Use of encrypted communication can be enforced for both WorkStation and WebStation access.
Communications | |
BACnet
|
BACnet/IP, port not configurable, default 47808
|
BACnet profile
|
BACnet Building Controller (B-BC), AMEV AS-B
|
BACnet certification
|
BTL Certification (BTL Listing
a
, WSPCert)
|
a) See the BTL Product Catalog for up-to-date details on BTL listed firmware revisions on BACnet International's homepage. | |
OPC UA Client
|
|
Profile group UACore 1.03
|
Core Client Facet, Base Client Behaviour Facet
a
, AddressSpace Lookup Client Facet, Attribute Read Client Facet
a
, Attribute Write Client Facet
a
, DataChange Subscriber Client Facet
a
, Method Client Facet, UA-TCP UA-SC UA-Binary, SecurityPolicy – Basic256, SecurityPolicy – Basic256Sha256, User Token – Anonymous Facet, User Token – User Name Password Client Facet, DataAccess Client Facet, Base Event Processing Client Facet, and Historical Access Client Facet.
|
a) Partly supported. See technical literature for more information. | |
Modbus
|
Modbus TCP, client and server
|
MQTT
|
MQTT over TLS, port configurable, default 8883
|
MQTT over TCP, port configurable, default 1883
|
|
MQTT over WebSocket Secure (WSS), port configurable, default 443
|
|
MQTT over WebSocket (WS), port configurable, default 80
|
|
TCP
|
Binary, port fixed, 4444
|
HTTP
|
Non-binary, port not configurable, default 80
|
HTTPS
|
Encrypted supporting TLS 1.3, 1.2, 1.1
a
, and 1.0
a
, port not configurable default 443
|
a) Disabled by default. | |
SMTP
|
Email sending, port configurable, default 25
|
SMTPS
|
Email sending, port configurable, default 587
|
Hardware compatibility | |
Fire detection panels
|
Esmi Sense FDP221
|
Esmi Sense FDP252
|
|
Esmi Sense FDP292
|
|
Field devices
|
Esmi Impresia range (ELC)
|
Esmi Intellia range (ALC)
|
|
Esmi Essentia range (ALC)
|
|
Esmi SLC range (SLC)
|
|
Conventional range (CLC)
|
|
Software bundles | |
Subscription plans – Standalone fire detection system | |
Essential plan 1 year on premise subscription duration Standalone
|
|
A single fire detection system, without any Enterprise Server.
|
FFSEFOPES00012
|
Enhanced plan 1 year on premise subscription duration Standalone
|
|
A single fire detection system, without any Enterprise Server.
|
FFSEFOPEH00012
|
Advanced plan 1 year on premise subscription duration Standalone
|
|
A single fire detection system, without any Enterprise Server.
|
FFSEFOPAD00012
|
Subscription plans – EcoStruxure BMS architecture | |
Essential plan 1 year on premise subscription duration FDP
|
|
1 fire detection system in EcoStruxure BMS architecture.
|
FFSEFOPES00212
a
|
a) Requires separate subscription plan for Enterprise Server(s), FFSEFOPES00112. | |
Enhanced plan 1 year on premise subscription duration FDP
|
|
1 fire detection system in EcoStruxure BMS architecture.
|
FFSEFOPEH00212
a
|
a) Requires separate subscription plan for Enterprise Server(s), FFSEFOPEH00112. | |
Advanced plan 1 year on premise subscription duration FDP
|
|
1 fire detection system in EcoStruxure BMS architecture.
|
FFSEFOPAD00212
a
|
a) Requires separate subscription plan for Enterprise Server(s), FFSEFOPAD00112. | |
Esmi Sense FDP fire system with Enterprise Server connection 1 year on premise subscription duration
|
|
Connects Esmi Sense FDP fire system to Enterprise Server.
|
|
1 fire detection system in EcoStruxure BMS architecture.
|
FFSEFOSFD00012
|
Subscription plans – Fire system scalability | |
Esmi Sense FDP panel in network count 1 year on premise subscription duration
|
|
1 Esmi Sense FDP fire detection panel in a fire detection system network (RS-485).
|
FFSEFOFDP00012
|
Add-on options | |
Client on premise 1 year subscription duration, EcoStruxure Fire Operation WebStation
|
|
For 1 concurrent user
|
FFSEFOCLN00012
|
Connected device 1 year on premise 10-pack FDP
|
|
Connect 10 devices over BACnet/IP or Modbus TCP/IP
|
FFSEFOCDE00012
|
Software requirements | |
External log storage PostgreSQL option
|
Supported versions of PostgreSQL (
www.postgresql.org
) with matching version of TimescaleDB extension (
www.timescale.com
).
|
Note: To use compression for trend data, TimescaleDB 2.11 or later is required.
|
|
Quality assurance testing has been performed by Schneider Electric with TimescaleDB and PostgreSQL installed natively in Windows 10, Windows Server 2012, 2016, and 2019. Other deployment scenarios have not been tested by Schneider Electric. | |
External log storage Microsoft SQL option
|
Microsoft SQL Server versions under full support by Microsoft (
www.microsoft.com
).
|
The following Microsoft SQL Server editions are supported: Enterprise, Standard, and Express. | |
External log storage AVEVA PI System option
|
PI Web API 2021 SP3 and database compatible with that version
|
Quality assurance testing has been performed by Schneider Electric with PI Web API 2021 SP3, and database compatible with that version, installed on Windows Server 2019. Other deployment scenarios have not been tested by Schneider Electric. |