Use the Basic tab to view and update basic properties of the option board.
Property |
Description |
Index |
Displays the index, which is a unique number set by the fire detection system. |
BoardType |
Displays the board type, for example ALC, IOC, or MCU. For more information, see O1891 EcoStruxure Fire Expert Configuration Manual . |
Status |
Displays the online/offline status. |