Use the Basic tab to view and update basic properties of the clean contact output.
Property |
Description |
IO function |
Displays the IO function. |
Contact description |
Displays the contact description. |
Index |
Displays the index, which is a unique number set by the fire detection system. |