Disabling a Loop Device or a Zone from a Graphic
You disable a loop device or a zone if you are going to perform maintenance work that might cause a false alarm.
Warning
|
COMPROMISED FUNCTIONALITY
If there is a risk for dust particles where smoke detection is used, attach dust covers to the detectors before you disable loop devices or zones related to fire detection and evacuation.
Comply with any applicable legislation, regulations, standards and/or guidelines regarding actions to be taken when parts of the fire detection system are unresponsive.
Enable the loop devices and zones again at the earliest opportunity.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
|
To disable a loop device or a zone from a graphic
In WorkStation or WebStation, in a graphic, click an enabled loop device or zone.
On the
Actions
menu, click the
Enable/Disable
button, which displays the current state (enabled) of the loop device/zone:
action_zoom_plus_stroke
If you want to disable the object and automatically enable it after a certain amount of time, click the
action_zoom_plus_stroke
button. Use the time selector
action_zoom_plus_stroke
to increase or decrease the number of hours from disabling to enabling the object.
Click the
Apply
button
action_zoom_plus_stroke
to disable the object.
The object is disabled and the updated state is visible in the graphic.
Fire Graphic Menus