earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation, WebStation
Functionalities: Basic Functionality, Graphics
12/11/2025

Disabling a Loop Device or a Zone from a Graphic

You disable a loop device or a zone if you are going to perform maintenance work that might cause a false alarm.

Warning Warning

COMPROMISED FUNCTIONALITY

  • If there is a risk for dust particles where smoke detection is used, attach dust covers to the detectors before you disable loop devices or zones related to fire detection and evacuation.

  • Comply with any applicable legislation, regulations, standards, and guidelines regarding actions to be taken when parts of the fire detection system are unresponsive.

  • Enable the loop devices and zones again at the earliest opportunity.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

To disable a loop device or a zone from a graphic
  1. In WorkStation or WebStation, in a graphic, click an enabled loop device or zone. On the Actions menu, click the multiselect icon

     
    action_zoom_plus_stroke
    to select several loop devices or zones. Use the selector
     
    action_zoom_plus_stroke
    to browse existing selections and click one of them.

  2. On the Actions menu, click the Disable option. If you want to disable the objects and automatically enable them after a certain amount of time, click the option Disable with auto-enable timer . Use the time selector

     
    action_zoom_plus_stroke
    to increase or decrease the number of hours from disabling to enabling the objects.

  3. Click the Apply button

     
    action_zoom_plus_stroke
    to disable the objects.

  4. Click Yes to execute the action, click No to cancel it.

The objects are disabled and their updated state is displayed in the graphic.

  • Fire Graphic Menus